Other Parts Discussed in Thread: SYSBIOS
Hello,
I installed the standalone versions of SYS BIOS and XDCtools (on Windows), to build an application without CCS. According to the SYS/BIOS 6.x Product Download Pages the current versions to use are SYS/BIOS 6.34.04.22 and XDCtools 3.24.05.48.
When I install these and try to compile a configuration (that was originally created using CCS) I get the following warnings:
Warning: xdc.cfg.INCOMPATIBLE_TARGET_VERSION: current target 'ti.targets.arm.elf.A8Fnv' [1,0,4.9,7] is not compatible with targets used to build the following packages
; package ti.sysbios.family.arm [in <...>/sysbios/packages/ti/sysbios/family/arm/] was built using 'ti.targets.arm.elf.A8Fnv' [1,0,5.0,1]
; package ti.sysbios [in <...>/sysbios/packages/ti/sysbios/] was built using 'ti.targets.arm.elf.A8Fnv' [1,0,5.0,1]
; package ti.sysbios.hal [in <...>/sysbios/packages/ti/sysbios/hal/] was built using 'ti.targets.arm.elf.A8Fnv' [1,0,5.0,1]
..........
and after this some more identical warning appear. When I checked the package.bld.xml files I also find the versions in there.
The command I use is:
<...>/xdctools/xs --xdcpath="<...>/sysbios/packages;" xdc.tools.configuro -o ./configPkg -c <...>/compiler -t ti.targets.arm.elf.A8Fnv -p ti.platforms.evmAM3359 -r release app.cfg
Can I use the generated files (with the warnings), or should I use a different combination of SYS BIOS and XDCtools?
(BTW: I tried versions SYS BIOS versions 6.34.03.19 and XDCtools version 3.24.6.63, but they give the same problem: the older SYS BIOS version also has version 1,0,5.0,1 and the new XDCtools still has version 1,0,4.9,7).
Regards,
Johan Borkhuis