Other Parts Discussed in Thread: SYSBIOS
Hi,
I am trying to modify the LEDs in board file (board-am335xevm.c). Presently it has configured for the GPIO_TO_PIN(1, 21), but we want to test the same functionlity for GPIO_TO_PIN(1,2).
We have modified the following:
#define BEAGLEBONE_USR1_LED GPIO_TO_PIN(1, 6)
#define BEAGLEBONE_USR2_LED GPIO_TO_PIN(1, 7)
#define BEAGLEBONE_USR3_LED GPIO_TO_PIN(1, 2)
#define BEAGLEBONE_USR4_LED GPIO_TO_PIN(1, 3)
static struct gpio_led bone_gpio_leds[] = {
{
.name = "beaglebone::usr0",
.default_trigger = "heartbeat",
.gpio = BEAGLEBONE_USR1_LED,
},
{
.name = "beaglebone::usr1",
.default_trigger = "mmc0",
.gpio = BEAGLEBONE_USR2_LED,
},
{
.name = "beaglebone::usr2",
.gpio = BEAGLEBONE_USR3_LED,
},
{
.name = "beaglebone::usr3",
.gpio = BEAGLEBONE_USR4_LED,
},
};
static struct gpio_led_platform_data bone_gpio_led_info = {
.leds = bone_gpio_leds,
.num_leds = ARRAY_SIZE(bone_gpio_leds),
};
static struct platform_device bone_leds_gpio = {
.name = "leds-gpio",
.id = -1,
.dev = {
.platform_data = &bone_gpio_led_info,
},
};
static struct pinmux_config bone_pin_mux[] = {
{"gpmc_ad6.gpio1_6", OMAP_MUX_MODE7 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA }, //LED1
{"gpmc_ad7.gpio1_7", OMAP_MUX_MODE7 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA }, //LED2
{"gpmc_ad2.gpio1_2", OMAP_MUX_MODE7 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA }, //LED3
{"gpmc_ad3.gpio1_3", OMAP_MUX_MODE7 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA }, //LED4
/* Grounding gpio1_6 (pin 3 Conn A) signals bone tester to start diag tests */
{"gpmc_ad6.gpio1_6", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT_PULLUP}, //chandu commented for b_cast_pin_MUX
{NULL, 0},
};
static void boneleds_init(int evm_id, int profile )
{
int err;
setup_pin_mux(bone_pin_mux);
err = platform_device_register(&bone_leds_gpio);
if (err)
pr_err("failed to register BeagleBone LEDS\n");
}
if (beaglebone_leds_free == 1) {
pr_info("Beaglebone: initializing onboard LEDs");
boneleds_init(0,0);
after updating pinmux with different pins i am not able to see /sys/class entry of these LEDs.
Please let me know what is the change i need to look into.