Other Parts Discussed in Thread: TPS65910A
I'm working on a design for a client that modifies the TMDSSK3358 evaluation board.
1. Our system will convert +24V supply to +5V to provide the equivalent of VBAT on the schematics. We would like the system to power up with out user intervention with the push button.
I saw the post (http://e2e.ti.com/support/arm/sitara_arm/f/791/t/235319.aspx) which describes a method of converting the eval board to automatic start (no push button). Essentially VBAT is connected to the PWRHOLD pin of the PMIC (TPS65910A3).
This method could be used in our system; but studying the documentation for the PMIC and AM335x, it seems preferable to use the AM335x PMIC_POWER_EN output to drive the PMIC PWRHOLD pin & initiate a "startup reason" for the PMIC power supplies.
Is it correct that this would make the push button on the PMIC PWRON pin unnecessary?
Is it a problem that PMIC_POWER_EN only reaches VRTC of 1.8V?
2. On the TMDSSK3358 schematic, the PMIC GPIO_CKSYNC pin is pulled up to VRTC. It seems that this pin should be pulled to the VDDIO selection (VAUX33).
Am I missing something?
Thanks for your time,
Russ