Hi,
I have a question regarding the USB module of OMAP-L138.
The above figure is from USB 2.0 Specification. I understand USB FS/LS host controller must be connected DP/DM to GND through 15kohm resistor.
Also, according to the data sheet of OMAP-L138, USB0_DM and USB0_DP signal has the IPD resistor.
My customer uses OMAP-L138 as host controller. And customer would like to connect the HID class keyboard. The speed are LS and FS.
In the above situation,
1) Does customer need to add any external resistors to USB line for connecting LS/FS Keyboard?
2) What is the value of IPD of OMAP-L138? Is it 15kohm?
3) Are there other requirements for HID class keyoboard connection?
Please advise me.
I appreciate your quick reply.
Best regards,
Michi