Other Parts Discussed in Thread: AM3715
Hi there!
Are there any Sitara devices that support 2GB Flash? This is for the development of an aircraft HMI.
Thanks!
Ari
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3715
Hi there!
Are there any Sitara devices that support 2GB Flash? This is for the development of an aircraft HMI.
Thanks!
Ari
Hi Biser,
Thanks for your reply! Would AM3715 be able to support 2GB NAND?
Ari
Thanks Biser. Could you clarify the below for me?
Eight independent GPMC chip-selects (gpmc_ncs0 to gpmc_ncs7) are available in the first quarter
(Q0) of the addressing space to access NOR/NAND flash and SRAM memories. The chip-selects have
a programmable start address and programmable size (16, 32, 64, or 128MB) in a total memory space
of 1GB.
Excerpt from the TRM of the AM3715.
Ari
Hi,
Yes it is possible and even more it can be interfaced. Attached document which explain about the interface used for NAND and NOR flash.8686.tn2919.pdf