This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 I2C slave boot



Per the Bootloader User Guide, to load tables into the C6678 in I2C slave mode we first send a six byte header: TTxx xx yy yy zz zz, where zz zz = boot option.

I want to verify that "boot option" in I2C slave mode is the same as in I2C master mode, i.e. 0 = Boot Parameter Table; 1 = Boot Table; 2 = Boot Configuration Table.

Is this correct?  I'm concerned some documentation seems to imply we can only send a Boot Table in I2C slave mode; but I want the option of doing a secondary boot using Ethernet or PCIe with the DDR3 enabled.