Other Parts Discussed in Thread: OMAP-L137
Hello,
I'm trying to configure the Ethernet interface on an OMAP-L137 evalutation board, but I cannot modify the content of the MACADDRHI register of the emac Module to set the MAC addresses of the device. Here is the code I use to initialize the Emac Module up to the initialization of the mac addresses :
void mdioInit() {
// setting the divider of the MDIO to reach a 1MHz clock (from 50MHz clock)
CSL_FINS(mdioRegs->CONTROL, MDIO_CONTROL_CLKDIV, 0x20);
// Enable the state machine
CSL_FINST(mdioRegs->CONTROL, MDIO_CONTROL_ENABLE, YES);
}
void emacModuleInit() {
// Select MII mode
// Open Permissions to SYSCFG Registers
_call_swi(ARM_PRIV_MODE_KEY);
CSL_FINS(sysRegs->KICK0R, SYSCFG_KICK0R_KICK0, KICK0_KEY);
CSL_FINS(sysRegs->KICK1R, SYSCFG_KICK1R_KICK1, KICK1_KEY);
// 1. If enabled, clear the device interrupt enable bits in the EMAC control module
// interrupt control registers CnRXTHRESHEN, CnRXEN, CnTXEN, and CnMISCEN.
CSL_FINS(emacCtlRegs->SOFTRESET, ECTL_SOFTRESET_RESET, 1);
// 2. Clear the MAC control register (MACCONTROL), receive control register
// (RXCONTROL), and transmit control register (TXCONTROL) (not necessary
// immediately after reset).
CSL_FINST(emacRegs->SOFTRESET, EMAC_SOFTRESET_SOFTRESET, RESET);
while (CSL_FEXT(emacRegs->SOFTRESET, EMAC_SOFTRESET_SOFTRESET) != 0)
;
delay(100 * infiniteTimerBitsPerMicroSecond);
mdioInit();
UINT16 tmpReg;
UINT64 endTimeout = readInfiniteTimer() + 3 * infiniteTimerBitsPerSecond;
do {
accessPHYregister(3, 1, FALSE, &tmpReg);
delay(100 * infiniteTimerBitsPerMicroSecond);
} while ((tmpReg & 0x4) == 0 && (endTimeout > readInfiniteTimer()));
if ((tmpReg & 0x4) == 0) {
return;
}
emacRegs->MACCONTROL = 0;
emacRegs->RXCONTROL = 0;
emacRegs->TXCONTROL = 0;
// 3. Initialize all 16 header descriptor pointer registers (RXnHDP and TXnHDP) to 0.
emacRegs->RX0HDP = 0;
emacRegs->RX1HDP = 0;
emacRegs->RX2HDP = 0;
emacRegs->RX3HDP = 0;
emacRegs->RX4HDP = 0;
emacRegs->RX5HDP = 0;
emacRegs->RX6HDP = 0;
emacRegs->RX7HDP = 0;
emacRegs->TX0HDP = 0;
emacRegs->TX1HDP = 0;
emacRegs->TX2HDP = 0;
emacRegs->TX3HDP = 0;
emacRegs->TX4HDP = 0;
emacRegs->TX5HDP = 0;
emacRegs->TX6HDP = 0;
emacRegs->TX7HDP = 0;
// 4. Clear all 36 statistics registers by writing 0 (not necessary immediately
// after reset).
emacRegs->RXGOODFRAMES = 0;
emacRegs->RXBCASTFRAMES = 0;
emacRegs->RXMCASTFRAMES = 0;
emacRegs->RXPAUSEFRAMES = 0;
emacRegs->RXCRCERRORS = 0;
emacRegs->RXALIGNCODEERRORS = 0;
emacRegs->RXOVERSIZED = 0;
emacRegs->RXJABBER = 0;
emacRegs->RXUNDERSIZED = 0;
emacRegs->RXFRAGMENTS = 0;
emacRegs->RXFILTERED = 0;
emacRegs->RXQOSFILTERED = 0;
emacRegs->RXOCTETS = 0;
emacRegs->TXGOODFRAMES = 0;
emacRegs->TXBCASTFRAMES = 0;
emacRegs->TXMCASTFRAMES = 0;
emacRegs->TXPAUSEFRAMES = 0;
emacRegs->TXDEFERRED = 0;
emacRegs->TXCOLLISION = 0;
emacRegs->TXSINGLECOLL = 0;
emacRegs->TXMULTICOLL = 0;
emacRegs->TXEXCESSIVECOLL = 0;
emacRegs->TXLATECOLL = 0;
emacRegs->TXUNDERRUN = 0;
emacRegs->TXCARRIERSENSE = 0;
emacRegs->TXOCTETS = 0;
emacRegs->FRAME64 = 0;
emacRegs->FRAME65T127 = 0;
emacRegs->FRAME128T255 = 0;
emacRegs->FRAME256T511 = 0;
emacRegs->FRAME512T1023 = 0;
emacRegs->FRAME1024TUP = 0;
emacRegs->NETOCTETS = 0;
emacRegs->RXSOFOVERRUNS = 0;
emacRegs->RXMOFOVERRUNS = 0;
emacRegs->RXDMAOVERRUNS = 0;
// 5. Setup the local Ethernet MAC address by programming the MAC index register
// (MACINDEX), MAC address high bytes register (MACADDRHI), and MAC address low
// bytes register (MACADDRLO). Be sure to program all eight MAC address registers
// - whether the receive channel is to be enabled or not.Duplicate the same MAC
// address across all unused channels. When using more than one receive channel,
// start with channel 0 and progress upwards.
// All eight addresses share the upper 40 bits. Only the lower byte is unique
// for each address. An address is written by first writing the address number
// (channel) into the MACINDEX register. The upper 32 bits of the address are
// then written to the MACADDRHI register, which is followed by writing the
// lower 16 bits of the address to the MACADDRLO register. Since all eight
// addresses share the upper 40 bits of the address, the MACADDRHI register
// only needs to be written the first time.
emacRegs->MACINDEX = 0x0;
CSL_FINS(emacRegs->MACADDRHI, EMAC_MACADDRHI_MACADDR5, 0x00);
CSL_FINS(emacRegs->MACADDRHI, EMAC_MACADDRHI_MACADDR4, 0x0E);
CSL_FINS(emacRegs->MACADDRHI, EMAC_MACADDRHI_MACADDR3, 0x99);
CSL_FINS(emacRegs->MACADDRHI, EMAC_MACADDRHI_MACADDR2, 0x02);
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,VALID);
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_MATCHFILT, MATCH);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_CHANNEL, 0);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 1;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 2;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 3;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 4;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 5;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 6;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
emacRegs->MACINDEX = 7;
CSL_FINST(emacRegs->MACADDRLO, EMAC_MACADDRLO_VALID,INVALID);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR1, 0xFE);
CSL_FINS(emacRegs->MACADDRLO, EMAC_MACADDRLO_MACADDR0, TDMA_DEVICE_NUMBER);
}
But the emacRegs->MACADDRHI is locked to 0x02385926 and even in Code Composer Studio I cannot modify this value.
What did I miss ?
Best regards
Arthur