Hi
Our system uses a DM648 at 864 MHz. We are trying to reduce power consumption, but didn't get much (400 mW) when we reduced the clock from 864 MHz (50% utilization) to 594 MHz (88% utilization).
What other things should we try to reduce the watts?
We are using 2 video ports, uart, emif and ddr2.
I have tried setting the unused peripherals (i.e. VLYNQ, SPI, HPI, the 3 unused vports, AMcBSPs....10 perripherals total) to disable state. This reduced power by about 100 mW. The spread sheet (http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=spraar5a) calculated about 200 mW. Its not near the reduction we need, but its something. Is the spreadsheet incorrect? Should we have got 200 mW?
Thanks