Hi Sirs,
I have an TI OMAP 5432 evm board, and i download GLSDK 6_01_00_01 for linux and u-boot source code.
I want to add eMMC HS200 flow in my uboot, but i have some question in CMD21 tuning flow
That is my tuning function. Refer to OMAP5432 RTM 24.5.1.2.4, SD104/HS200 DLL Tuning Procedure.
I always hang on step 3(MMCHS_DLL[0] all always unlock!!), after i setting MMCHS_AC12[22] ET to 0x1.
By the way, in the step one, the MMCHS_DLL regester value is 0x80000000,
Thanks.
with Best Regards,
ShinFu