Other Parts Discussed in Thread: OMAP-L137, OMAPL138, OMAP-L138, TMDSLCDK138
Hi,
I'm trying to run an IPC IO example on a OMAP L138 LCDK using CCSv5.2.1.00018, on the DSP core (C674x), but when I try to debug, I have the following error message : "C674X_0: Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.747.0)"
The same example works fine on the ARM core.
IPC version is 1.24.3.32, and the RTSC platform I selected is ti.platforms.evmOMAPL138 (can't find any LCDKOMAPL138 - not quite sure the problem is there as the same platform works fine for the ARM core); I use the Spectrum Digital XDS100v2 USB emulator.
I went through the forum but couldn't find relevant topics, any help would be appreciated
thks
Philippe