This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Procedure to run aif2CpriFastCMK2KTestProject on C66x

Hi,

I am using MCSDK version 3.00.02.14

I am trying to run aif2CpriFastCMK2KTestProject in Dual EVM setup. The internal loopback test is passing.

I am not clear with the test procedure. I am going to break my queries into points.

1. The predefined symbols in the project are as listed below. Of this, which one should be used and what value they should carry to tun aif2CpriFastCMK2KTestProject in Dual EVM setup?

EVM_TYPE=6

LOOPBACK

DEVICE_K2K

LTE_RATE=60

USESYSBIOS

SIMULATOR_SUPPORT

2. A part of the test procedure in the test is as below. Can someone please explain what does it mean ?

* Pre-processing constants of interest:
* - EVM_TYPE: 1 - internal loopback or EVM DSP1 (dual EVM setup), 2 - EVM DSP2 (dual EVM setup), 3 - SCBP            DSP1, 5 - EVM6614 (Cpri Relay setup), (0 - old Lyrtech C6670 EVM)
* - LOOPBACK: selects internal loopback mode (SerDes level, AIF2 SW trigger)

3. There are two build configurations K2K_LBACK & K2K_LBACK_BE, which build configuration to use?

4. I am running the test but it is hanging in the middle. The test log is as below.

Beginning AIF2 LTE RF tests:
test: LTE_20MHZ_FASTCM
AIF CPRI mode
link 0 runs at 4x rate
outbound data type: DL
outbound data width: 15 bit
inbound data type: DL
inbound data width: 15 bit
link 1 is disabled
link 2 is disabled
link 3 is disabled
link 4 is disabled
link 5 is disabled

Please help

Regards

Pradeep