This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C674x maximum SPI master rate



Hi,

I'm trying to find out if I can use a C674x to ingest data from an ADC that outputs on a SPI bus at 100 MHz. The processor would be the SPI Master. Can any of these DSPs (or others) handle this rate or is an FPGA my only option? I'm trying to find a processor <2 W.

Thanks!

  • Hi Jason,

    The maximum SPI clock frequency supported by C674x device is 50MHz or 3P whichever is greater

    P=SYSCLK2 period

    Please refer the datasheet for more details page no 165 General Timing Requirements for SPI0 Master Modes.

    Regards

    Antony

    • --------------------------------------------------------------------------------------------------------
      Please click the Verify Answer button on this post if it answers your question.
      --------------------------------------------------------------------------------------------------------