Hi Titus,
Thank you very much for reply,
You are right, i checked the hardware and found that MDC line was not connected to the phychip.
I connected MDC line with wire(manually) and guess what phy is getting detected!! :)
I will get that line connected with hardware guys and i will also get other interface checked and then test tftp from u-boot.
Here is boot log,
In: serial
Out: serial
Err: serial
DIR45 0Xc8014020
OUT_DATA45 0X11000040
SET_DATA45 0X11000040
CLR_DATA45 0X11000040
Delay for 10 seconds...
Delay done
Mux3 value 0x1affff
ARM Clock :- 297MHz
DDR Clock :- 270MHz
davinci_eth_phy_detect(), ALIVE = 0x00000002
Ethernet PHY: DP83848 @ 0x01
Thank you,
Regards,
Ankur