Other Parts Discussed in Thread: OMAPL138
Hi,
1. I would like to know if i can use cppi dma in RNDIS mode to realize a USB mass storage device in rx. I see the startware use transparent mode for rx. But transparent mode would cause a number of interrupts in receiving. Is there any examples i can take as a reference?
2. I read the spruh77a carefully and found that cppi dma would trigger the interrupt only after receiving the whole packet, then i can offload the whole packet once in the isr. Do i have any misunderstanding in cppi dma's RNDIS mode?
3. I've not used the cppi dma before, and CPU take the responsibility to offload data from fifo after a WRITE10 command, but only 0x400 bytes at most can be received at one time. It seems that a buffer overrun occurs when the packet length is larger than 0x400 bytes. Dose this trouble can be avoid by using cppi dma?
Huang