This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6670 SPI NOR boot



Hello, I have a board with C6670 connected to NOR flash on SPI.Design and flash chip is identical to C6670 EVM. I want the DSP to boot from the flash on POR.I used the norwriter as instructed in the readme file. BOOTMODE 0:12 configured according to data manual for spi boot. Runing the norwriter was sucsesfull but the DSP deos not boot after POR. Is there anything else I need to do? Best regards, Ronen
  • Hi Ronengi, 

    Have you tried to place the code in MSMC and see if the boot completes?

    Have you verified the SPI writes to the NOR flash by reading back the data.

    Can you probe the SPI data lines and check if you see data on the lines when the clock is provided?

    Are you using the default SPI parameter table to boot the device?

    Thanks.

  • Hi Rajasekaran

    1. Didn't try MSMC

    2. Yes, verified.

    3. There is data on the lines constantly

    4. What are the default parameters? How do I generate this parameter table and combine with my code?.

    Best,

    Ronen

  • Tried MSMC, still not working.

    BOOTCOMPLETE 0. DEVSTAT: D40D

    Best,

    Ronen

  • Hi Ronen,

    Can you please help us understand your design a little better. Is your board designed similar to the C6670 EVM. Does your board implement a IBL and the boot from the SPI NOR. Where is your application being loaded. Does your boot image initilailize DDR and place code in it.? Have you tried to boot the C6670 EVM using SPI NOR boot. Here is an working example of how to convert an .out file to boottable that you can boot on C6670/C6678 device and document of how to create the boot image.

    0675.SPI_Bootloader.zip

    8015.Booting_from_SPI NOR_C6678.pdf

    Please give this a try and let us know if you had any issues.

    Regards,

    Rahul

  • Hi Rahul, My board has C6670 connected to SPI NOR FLASH, same flash and design as in the EVM. No IBL and no DDR load, code should load to L2RAM only. I'm just confused about creating the boot image for the NOR since all the exaples are for creating the boot on the evm which iplements ibl. Do I have to use ibl? Best, Ronen
  • Hi Rahul,

    Thank you for the info and example. I did that but it looks like the RBL is not completing the boot process.

    What is the exact process for making a boot image with no IBL involved? My code is compiled as little endian and I used the ccs2bin -swap command to change it to big endian for the RBL as instructed. Is it the correct way to do it?

    Any other suggestions?

    Best,

    Ronen 

  • DId you try the example on the EVM?  Did you use the ROM SPI boot settings from the wiki page

    http://processors.wiki.ti.com/index.php/TMDXEVM6670L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings

    Please mention the value of the program counter and the DEVSTAT register. I want to confirm that you have set the boot pins to SPI boot and the RBL is executing code for SPI. 

    Regards,

    Rahul

  • Hi,

    The boot is working after I made changes to the parameter table file (*.map).

    Changed mode from 0 to 1.

    I am not sure about the parameters in the 8.rmd file.

    This is what I'm using for my program:

    ARC1_CHA.out
    -a
    -boot
    -e _c_int00

    ROMS
    {
       ROM1:  org = 0x0C000000, length = 0x200000, memwidth = 32, romwidth = 32
              files = { spiboot.btbl }
    }  

    What do I need to change in order to work with L2SRAM?

    Thanks,

    Ronen

  • Ronen,

    Good to know you are making progress with the example provided. I am not the hex6x utility expert so you may be able to find an answer to this on the COmpiler forums. THe hex6x utility is documented with the ROM directives in the C6000 assembly language tools documentation that you will find under CCSv5/tools/compiler/c6000_x.x.x/doc in section 11. 

    My understanding is the ROM origin address in the RMD file is the location where the hex6x starts looking for sections in your application binary and then it reads the .out until the end of the length specified in the rmd file.

    Change this address to base of L2SRAM if your application places code in L2 memory. Add add sufficient length to cover all sections of your application.

    Regards,

    Rahul

    Regards,

    Rahul

  • Hi Rahul,

    Thank you for your help.

    Best,

    Ronen

  • Hi Rahul,

    Sorry for interrupting you.

    I have a question about SPI_Bootloader.zip which you attached to this post.
    There nysh.spi.map inside this zip file.

    My question is about the nysh.spi.map.
    In nysh.spi.map, there are following parameter for PLL.
    ===============================
    * sw_pll_prediv
    * sw_pll_mult
    * sw_pll_postdiv
    * sw_pll_flags
    ===============================
    Which PLL register does these parameter affect to?

    And I want to speed up the SPI bus frequency.
    At default it looks like the RBL will setup the SPI bus frequency to 20MHz..
    For example, if I want to setup to 50.5MHz, is the following configuration correct?
    ======================
    * bus_freq_mhz = 50
    * bus_freq_khz = 500
    ======================

    best regards,
    g.f.

  • g.f. said:
    In nysh.spi.map, there are following parameter for PLL.
    ===============================
    * sw_pll_prediv
    * sw_pll_mult
    * sw_pll_postdiv
    * sw_pll_flags
    ===============================
    Which PLL register does these parameter affect to?

    The above software flags in the nysh.map file are used to configure the main PLL on C66x device. These registers will primarily configure PLL_CTL , PREDIV, PLLM registers using the PLL initialization sequence specified in the PLL USer Guide. 

    To see the complete  list of PLL registers these parameters impact please take a look at the hwPllsetPll function in pll.c file in the Gauss boot ROM source(hw/pll directory). The Gauss boot ROM source is provided on the wiki page below:

    http://processors.wiki.ti.com/index.php/Keystone_Device_Architecture#Keystone_ROM_Boot_Examples_and_Reference_code

    g.f. said:
    And I want to speed up the SPI bus frequency.
    At default it looks like the RBL will setup the SPI bus frequency to 20MHz..
    For example, if I want to setup to 50.5MHz, is the following configuration correct?
    ======================
    * bus_freq_mhz = 50
    * bus_freq_khz = 500
    ======================

    The bus_freq_mhz and bus_freq_khz configure the busFreqMhz and busFreqKhz parameter  of the boot parameter table for SPI boot. If you look into the tiboot.h file for the ROM, you can see the usage specified as shown below

    UINT16 busFreqMhz; /* The speed of the SPI bus, the megahertz portion */
    UINT16 busFreqKhz; /* The KHz portion of the bus frequency. A frequency of 1.5 MHz would have the value 5 here */

    So you are right to configure it to 50.5 Mhz  you should set these using the settings that you have mentioned in your post.

    Regards,

    Rahul

  • Hi Rahul,

    Thank you so much for the reply.

    I checked the boot ROM source code. From the source code, I understood that
    swi_pll_prediv will affect to MAINPLLCTL0.PLLDIV and
    swi_pll_mult will affect to MAINPLLCTL0.PLLM.
    I guess there is no register for sw_pll_postdiv in C6670.

    By the way, I'm able to get SPI bus clock(10.5MHz) which I expected by configuring the
    parameter as follow:
    (I checked the clock by using oscilloscope)
    *sw_pll_prediv = 1
    *sw_pll_mult = 32
    *sw_pll_flags = 1

    *bus_freq_mhz = 10
    *bus_freq_khz = 500

    But when I checked the Main PLL register from CCSv5 memory browser,
    the PLL_Mult and PLL_DIV bit value was set to zero.
    Do you know why it was set to zero?

    best regards,
    g.f.

  • The main PLL stays in bypass mode for no-boot, SPI, and I2C boot. For other boot modes, a PLL initialization sequence executes inside the boot ROM to configure the main PLL in PLL mode.

    Regards,

    Rahul

  • Hi Rahul,

    Thank you for the reply.

    I understood that PLL is in bypass mode if SPI/I2C boot are used.
    But I thought if setting the pll parameter in Boot parameter table,
    RBL will first read this table from SPI NOR flash to internal memory(L2) and
    then set the PLL controller to the expected value.
    So, is this understanding wrong? Then why there are pll parameter in Boot parameter table?

    Do you mean that PLL is in bypass mode and RBL won't change if SPI boot is used,
    but RBL will change SPI bus frequency to expected speed?

    In C6670EVM input clock is 122.88MHz, so that CorePac0 is running at 122.88MHz(bypassed)
    and SPI module clock are 20.48MHz. So, is 20.48MHz the maximum SPI bus frequency in EVM SPI boot mode?

    best regards,
    g.f.

  • Hi Rahul,

    I'm sorry for asking again but
    can you please reply to my last question?

    best regards,
    g.f.