This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

JPEG Encoder in DM365 support 5M resolutin or not?

Greetings,

As the jpeg encoder in dm365 noticed, the Images with resolutions up to (Horizontal MCUsize * 1024)*(Vertical MCU size * 1024) pixels can be encoded. This is the theoretical maximum; however, only images up to 10Mpixels have been tested.

But in my programme, I found that if width is bigger than 2048, then the image encoder output are interlacing color bars. Does that means the Horizontal MCUsize here means 2? The coder performance normal under other lower resolution. But the JPEG datasheet said that 10M pixels have been tested.

or the value of dynParams.numAU in the dynParams struct should be set to a proper value?

Best regards;