Other Parts Discussed in Thread: AM3359
Hello
We use the ICE board with TI chip AM3359 as a reference design for the EtherCat slave together with the twincat master.
In order to understand the limitation of EtherCat data transfer rate we did the following :
1) on the function void APPL_Application(void) we use a counter to increment the analog input port (every 10 ms ) and we record the data on the EtherCat line by using the wiershark sniffer we saw that if the counter increment every 10ms we did not lose any data , but if the counter rate is less than 10 MS we start to loos data .
Is it possible? We know that the EtherCat can transfer data on much higher speed (even 4khz)
How can we speed the data transfer by using this stack? do we need to change something on the configuration ?
thank you
Tsachy
Thank you
Tsachy