Does anyone have instructions or know if it's possible to build and use Qt 5.x on this development kit? Denix (on the #arago IRC channel) suggested I build an "arago-qt5-test-image", which yielded an image with some Qt5 libraries on it, but I haven't successfully run a Qt5 application yet as I'm working on getting the Graphics SDK to build right now.
I'm also wondering about the status of that arago-qt5-test-image - is this something still under development? It seems that Qt5 is experimental on this platform.