i am using am335x starter kit with ccsv5 and sdk7. when executing ifconfig command the inet address is missing. pls help.
root@am335x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:18:31:E7:A3:50
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:644 (644.0 B)
Interrupt:56
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:110 errors:0 dropped:0 overruns:0 frame:0
TX packets:110 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:185131 (180.7 KiB) TX bytes:185131 (180.7 KiB)
Thanks
Jawahar Krishnamoorthi