Hi,
does anyone know, if there is a windows CE porting for the OMAP-L137 / OMAP-L138?
Is there something available or planned at TI? In best case a starter kit...
Regards,
Joe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Based on this slide it looks like there should be a WinCE BSP sometime this quarter, though I have no details as to what it will contain or where it will come from yet, I will see what else I can find and post back here if I come across further information.
Hi Joachim,
The WinCE release for OMAP-L1 is predicted for end if May/2010.
Hi Mariana,
is there already a WinCE reference design available? I asume there will be also a starter kit?
Regards, Joe
I do not have this information yet, but I believe that the same starter kit from spectrum for Linux will be used.
CE6 R3 BSP available here http://support.mpcdata.com; reference design is available from Logic PD (L138) or Spectrum (L137).
Claus