This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6655] SPI 5-pin boot mode

Hi,

My customer spotted the old 5-pin mode in the C6655 datasheet,  although the SPI peripheral only support 4-pin or 3-pin mode.

SPRS814A—August 2012 , page 32 it is stated that the SPI mode either can be using 4 or 5 pins – which are these?

Normally the SPI interface is 3 or 4 pins, where 4 is the most common used: MISO, MOSI, CLK and CS#.

Please clarify.

/Magnus Aman