hi all:
I use the c6678 evm to run H264 transcode, but when it recv data faild from tftp, below is the tftp log:
Connection received from 192.168.200.100 on port 32768 [21/10 12:00:27.349]
Read request for file <airshow_p1280x720.264>. Mode octet [21/10 12:00:27.349]
OACK: <blksize=1460,> [21/10 12:00:27.349]
Using local port 51611 [21/10 12:00:27.349]
TIMEOUT waiting for Ack block #0 [21/10 12:00:42.414]
Connection received from 192.168.200.100 on port 32768 [21/10 12:13:49.801]
Unexpected request 5 from peer [21/10 12:13:49.801]
Returning EBADOP to Peer [21/10 12:13:49.801]
I use the demo path is :C:\ti\mcsdk_video_2_1_0_8\examples\transcode, after I build it, I follow the wiki step which
is http://processors.wiki.ti.com/index.php/MCSDK_VIDEO_2.1_CODEC_TEST_FW_User_Guide.
Is anything wrong?
Best Regards,
Si