This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355 AAC Encode Issue

Hi,

Our customer implemented AAC encoder on DM355 platform. Under 80% of ARM working ratio, audio mute for a few minutes sometimes happens in the AAC encoded stream. They confirmed input audio source correctly comes in without discontinuity.  The customer asked us following questions. It would be helpful if they are clarified.

Q1. Was similar issue reported ?

Q2. What is supposed as the root cause?

Q3. The customer is suspecting mute function is working wihtout intention during encoding/decoding. In ordinary case, what  condition is required to execute mute function?

 

Best regards,

Kojima