If I'm running Xmit and Rcv synchronously off the xmit clocks, frame sync, does it matter what I set the fields in RCLKCHK to? If so, and my xmit clocks are all derived from AUXCLK, then I don't understand the RPS description, which seems to suggest that RPS is the divider *from the McASP system clock (SYSCLK2?), but it doesn't describe what "check prescalar" means. It seems that it will be used to determine a receive clock error, but I'm not sure how.
I suppose I'd like know 1) do I care if I'm running synchronously and 2) how is it used (whether I care or not).