hi,
Our custom board PCB about DDR3 layout is
Byte 0 | Byte 1 | Byte 2 | Byte 3 | ||
DDR0 | CK trace | 2.6 | 2.6 | 3.6 | 3.6 |
DQS trace | 1.4 | 1.63 | 1.07 | 0.92 | |
DDR1 | CK trace | 2.56 | 2.56 | 3.56 | 3.56 |
DQS trace | 1.62 | 1.17 | 1.26 | 0.98 |
wether the Parameters are within the allowable range or not ,We use simulation of CCS to get WR DQS,RD DQS,RD DQS GATE,WR DATA ,
we make ubootall,But, when we load the uboot .min.nand and uboot.bin to my custom board , and power up the board ,but uart has not any information.
Could you help me?
Thanks in advances.
Best Regards,
stone