Hi, i saw am335x technical reference manual. in chapter 26, described Initialization. i understand LCD_DATA 0-15 are sysboot pin, pulldown or pullup will correspond to relative boot sequence.e.g 0100000000111100 is for MMC1,MMC0, UART0, USB0 booting. also, each pad has pad control registers to enable internal pull down/pull up. so,
1 what's the default config for pad control registers of LCD_DATA 0-15?
2 can i eliminate the external pull down/pull up resistors for sysboot?
moreover, there are control_status Register, bit 0-7 and 16-23 response to sysboot 0-15,
3 what's the default config on control_status Register?
4 how can i got 0100000000111100 for MMC1,MMC0, UART0, USB0 booting sequence by Software without set pull down/ pull up resistors by Hardware in the first initialization? is it possible?
many thanks.