Other Parts Discussed in Thread: SYSBIOS, AM3359
Hi,
I've just got my new dev kit AM335x ICE v2. I'm trying to flash a bootloader and/or an application into the onboard SPI flash via CCS. When I launch target configuration and I select GEL from "C:\ti\am335x_sysbios_ind_sdk_1.1.0.6\sdk\tools\gel\ICE\TMDXICE3359.gel". Once I run the "AM3359_ICE_Initialization" script, seems no problem in the console, but when I test the DDR3, it failed. I look inside the gel file, I see that the script is coded to initialize DDR2 and not DDR3. Is someone have the GEL file build for the new dev kit AM33x ICE V2 ?
Thanks in advance.
Eric