Other Parts Discussed in Thread: TMS320F28075, TMS320F28069, CONTROLSUITE
Hi. I'm using the 28075 controlCard and CCSv6.10. I have been doing the TI-RTOS labs from Eric Wilbur's workshop. I did all of the labs using a 28069 controlStick, and everything worked great. Now, changing the device to the 28075, I'm having problems.
In particular, I get a linker error telling me that the program won't fit into memory, and that the codestart section is too small.
"../TMS320F28075.cmd", line 103: error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section "codestart" size 0x2 page 0. Available memory ranges:
BEGIN size: 0x2 unused: 0x0 max hole: 0x0
I did the basic hello_world project for the 28075 that came with controlSuite, but that was designed for the 28075. The project that I'm trying to make work now is the blink_C28x_TASK project from Eric Wilbur's workshop. This was originally intended for the 28069, and I swapped TMS320F28075.cmd in place of the TMS320F28069.cmd file.
I've been reading other posts, but nothing I found seems to answer my question. Sorry if this has been answered already.
Thanks
Justin