Other Parts Discussed in Thread: OMAP-L138, AM1808
Hi,
My issue is how to set the block number of the NAND flash where the SFH program (v2.40) should store u-boot.bin.
My NAND partitioning is
#: name size offset mask_flags
- 0: u-boot_env 0x00020000 0x00000000 0
- 1: ubl 0x00020000 0x00020000 0
- 2: spare 0x00040000 0x00040000 0
- 3: u-boot 0x00080000 0x00080000 0
- 4: kernel 0x00700000 0x00100000 0
- 5: rootfs 0x0f800000 0x00800000 0
- 6: archive 0x10000000 0x10000000 0
Then I guess that 4 is the correct block number to use (offsets from 80000 to 100000)
Running the SFH command
sfh_OMAP-L138.exe -flash ubl_AM1808_NAND.bin u-boot.bin -targetType AM1808 -flashType NAND -p COM1 -baud 115200 -v -appFlashBlock 4
the u-boot.bin is actually stored at block 6 (look at the attachment)
Can anybody help ? Is it a bug of the SFH tool ?
Gabriele