Other Parts Discussed in Thread: OMAPL138
Hello,
I'm tailoring kernel to a custom OMAPL138 board whic is a mixture of LCDK and LogicPD' SOM. External flash is connected to SPI1 and is of type M25P64.
While booting m25p80 is detected and in also in /dev folder, as can be seen in attached screenshots.
When I try to make partitions and press "write" in fdisk, kernel is crashing
I'm using mcsdk_1_01_00_02 linux-3.3-psp03.22.00.06.sdk and running it with NFS now. Kernel code is based on "board-da-evm.c" with modifications to da850.c .
Could someone please assist me a bit with this issue.
risto