Dear Team,
Is there any restriction to use GPIO3_14 as input?
my customer is using GPIO3_14 pin for SD card detection by connecting it to 'cd' of SD card connector, but they could not get any input when SD card was inserted. When other GPIO was used for this, there was no issue. And when they set GPIO3_14 as output, there was no issue and they found output change also.
I requested to check GPIO initialization and pinmux setting, but they confirmed there was no issue found.
Is there any restriction to use GPIO3_14 as input?
In HW, they connect 10kohm pullup register.
Thanks and Best Regards,
SI.