This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SimpleLink CC3200 WiFi Package driver

Other Parts Discussed in Thread: CC3200, CC3200SDK, CC3100

Hi IT,

When will you provide a driver for the CC3200 so that we can use it in TI-RTOS XDC config tool.

Basically, I have newest drivers and CC3200SDK and simplelink. An empty TI-RTOS project and when enabling the WiFi driver in the XDC config tool (.cfg) I can only choose the 3100 from the device list!

This is a similar problem but does not answer the problem: LINK

Also, I have done this: LINK

I can see the problem is that the driver for the CC3200 is not included in the SimpleLink SDK. They should be here:

C:\ti\tirtos_simplelink_2_13_01_09\packages\ti\drivers\wifi

But only the CC3100 driver is to be found there!

That being said, let's say it was there. Then I need an example on how to configure and use it in TI-RTOS. Section 5.17 in the in the TI-RTOS user guide v2.12 is not that helpfull.

Please help.

Also, the CC3200SDK-SERVICEPACK-BETA cannot be downloaded due to some error. So I'm stuck! I basically have a project that needs to be delivered and I've selected TI as the vendor. Please don't let me down.

Kind regards

Anders Dam Kofoed