Other Parts Discussed in Thread: AM5728
I have some questions regarding the DRA7xx DDR3 controller initialization over JTAG Emulation.
Is it possible to initialize the controller properly without the CPU, that is can I hold the CPU in RESET and configure the DDR3 controller only over JTAG emulation ?
As far as I know from the TRM one cannot initialize the DDR3 memory chip/device with discrete COMMANDS (like NOP, PRE-ALL and so on) because this automatically is done by the DDR3 controller. Is there a possibility to see/debug which action of the 50-100 initialize steps fails ?
thanks in advance,
Peter