This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

initial booting of DM365 chip question

Hello.  My name is David Coburn.

In regard to a completely new board design.  When the board arrives is it possible to load an External Nor Flash hanging off the EMIF such that you can boot from it on the next power up? 

If not, then is the only solution to have the Nor Flash pre-programmed before you lay it on the board?  (assuming that we are limiting the conversation to booting from Nor Flash.  I do believe that it is possible to boot from a SD card via the MMC port using the ARM ROM Bootloader..  Is this correct?

thank you,

david