Other Parts Discussed in Thread: OMAP-L138
Hi, everyone:
I use the RTFS system to read and write SATA on the OMAP-L138 board. And I use bios_5_41_13_42, rtfs_1_10_02_32, pspdrivers_01_30_01.
My code stuck in ATA_DrvInit() function while it is working fine with RTFS example. After debugging I found that it is stuck in ATA_SubmitIdentify() function.
In the ATA_SubmitIdentify() function, there are a section of codes:
pReq -> Retry = 10u;
ATA_SubmitReq (pDevice, pReq);
while (pReq -> Retry != 0)
{
//PAL_osWaitMsecs (1u);
m_delay(1u);
//pReq -> Retry--;
}
And the m_delay function:
void m_delay( Uint32 msecDelay)
{
volatile Uint32 i,j;
// TSK_sleep(msecDelay);
for(i=0; i<msecDelay; ++i)
for(j=0; j<0x1fff; ++j); //TODO ???
}
If I run straightly, the program will enter infinite loop in the m_delay function. But if I abandoned the “//” before “pReq -> Retry--;”, and set a breakpoint before “while (pReq -> Retry != 0)”, the ATA_SubmitIdentify() function could go successfully and then ATA_driver could be Initialized successfully.
So how does the variable pReq -> Retry be changed? Could you please tell me why it is like this here and how I should configure here?
Please help me. Thanks a lot!
Best wishes
Samantha