This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BBB power consumption

Other Parts Discussed in Thread: AM3358, TPS65217

Dear TI

for the BBB has sitara AM3358 processor the data sheet says it can operate in one of these clock frequencies 600 MHz 800 MHz 1000 MHz 

Questions:

1). is there a way to step down the clock frequency bellow 50 Mhz the idea is to save power i know there is a sleep mode but our requirement is not to keep in sleep mode at all rather clock the frequency very low so that it consumes very less power.

2) is there a way to measure the total power consumed by the complete BBB hardware not by using multimeter but by using an IC with i2C interface so that the processor just reads the total power consumed.

Regards

Nick