If I am not using the USB or SATA functions, can I just ground the USB & SATA power pins or do I need to tie them to thier respective power rails?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I am not using the USB or SATA functions, can I just ground the USB & SATA power pins or do I need to tie them to thier respective power rails?
We have a schematic checklist which addresses what to do with the unused pins. This information will also be in the next revision of the datasheet.
http://processors.wiki.ti.com/index.php/OMAP-L1x_Schematic_Review_Checklist
Jeff
That is great, thanks. In the right column of the USB table under "if not used", I assume the title was suppose to be When USB1 is not used. Is that true?
I just noticed that the list of devices that the schematic checklist applies (near the top of the checklist) does not include the TMS320C6748 which is the part I am using. Is there one for my device?
For the USB table, I believe the last column should be "When USB0 is used, and USB1 is not used".
This should apply to the C6748 as well. I'll send this feedback to the wiki owner to get that updated.
- Christina