Hi,
I have questions about AM3357 ISDK and TLK105L.
In my customer's board there are two TLK105L for IN and OUT.
Each TLK105 are connected to AM3357 PRU.
They are using AM3357 PROFIBNET protocol as SLAVE and they are using ISDK v1.1.0.9.
They are having following issue right now.
//////////////////////////////////////////////////////////////
One TLK105L(IN) is connected to PROFINET Master and LED_LINK are blinking fine.
Other TLK105L(OUT) are not connected to anything but LED_LINK are also blinking.
We don't know why.
//////////////////////////////////////////////////////////////
For above issue, my customer have following questions.
Q1.When communication with PROFINET, who will judge the "Linkup"?
Is it pr1_mii<0:1>_rxlink of AM335x PRU or TLK105L register?
Q2.In customer board, TLK105L LED_LINK pin are connected to pr1_mii<0:1>_rxlink of AM335x.
Do I must connect LED_LINK to pr1_mii<0:1>_rxlink when using PROFINET communication?
Q3.When will TLK105L LED_LINK will get ON or blinking?
Is it only "Linkup" and during LAN communication?
Does LED get ON or blinking when AM3357 transmit the data?
best regards,
g.f.