Hi,
I have a question about C6654 GPIO.
We are going to use GPIO[31:16].
In Keystone GPIO user guide(sprugv1), each registers seems it could only configure GPIO[15:0].
I guess each registers bit[15:0] are correspond to GPIO[15:0] and bit[31:16] are reserved.
So, how to configure GPIO[31:16] ?
I guess each registers bit[31:16] are not reserved and it's correspond to GPIO[31:16], is it correct?
best regards,
g.f.