Other Parts Discussed in Thread: TMS320F2812
Hi,
I want to use the wonderful functionalities UIA provides. This is mainly to get time my application on SYS/BIOS. These are the details of my configuration
SYS/BIOS: 6.37.5.35
DSP: TMS320F2812
XDCtools : 3.25.6.96
System Analyzer: Installed but cannot find the version.
Code composer studio: 6.1.0
The problem I have is:
1) After checking the box on UIA in the RTSC tab of properties it does not show up in the XGCONF of the .cfg as mentioned in SPRUH43B
2) Is there an updated version of SPRUH43B. It will be great if there is some reading material present for the processor in the question.
Your help is highly appreciated.
Thanks & Regards,
Nikhil Kotian.