-
Hi,
I have few doubts over usage of vlan support feature in NDK.
I have gone through section A.16. I understand that VLANAddDevice() is to be used to create a vlan with specific ID for a specified interface.
This is the approach we are following :-
1) add CFGTAG_IPNET entry in NDK for interface 1 and setup IP address manually to the specified interface
2) VLANInit()
3) NC_NetStart invocation
4) VLANAddDevice() for the same interface and vlan ID 2 with some priority.
5) Bind socket to that IPThis leads to creation of new interface 2 having vlan ID 2 configured (eth0:2). We have specified interface 1 as argument to VLANAddDevice().
Is this behavior expected? We intended vlan tagging to be configured for interface 1.
Please send a test project showcasing vlan support in NDK on c6678 EVM.Regards,
Rajesh Teli
- NDK 2.21.0.32
- DSP/BIOS 6.35.04.50
- C6678