This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66ak2l06 DFE lane

Other Parts Discussed in Thread: 66AK2L06

Is it possible to connect more than one ADC Chip to a lane?

example:in 66ak2l06 there are 4 lanes,can i connect them to 16 ADCs,(4 ADCs for each lane) and control the timing with DFE GPIO?

THANKS

  • We have assigned this thread to experts and they will get back to you. Thank you for your patience.
  • The JESD interface as part of the 66ak2l06, has 4 lanes, 2 links. It supports JESD parameters of
    L=1,2,4; M=1,2,4,8; F = 2,4,8; S = 1; HD=0
    There are quad-data converters that connect to 1 JESD lane, typically the limitation here is the number of transmit and receive streams.
    Please review the DFE User Guide (spruhx8a.pdf ) there are 1,2, or 4 transmit streams, and 1, 2, 3, 4, or 5 receive streams. There is a new demonstration (demo) under development to process 8 real ADCs within the DFE. So although we could connect the (4) quad ADCs, there is not a signal processing solution to utilize 16 Rx streams.
    Regards,
    Joe Quintal