Sorry if this is the wrong place to ask this question, but in any case,
On the LCDK schematic the OMAP-L138 power section shows that pins VssA_USB0 and Vssa33_USB0 are not connected even though USB0_VDDA33 is connected to VCC_3V3D. I tried to find a reason for these two pins to be disconnected on the datasheet but couldn't. I have used USB0 fine actually (it works), just interested to know why these two are disconnected?.
Thank you,