Other Parts Discussed in Thread: DM3730
Hi,
In my design I am using a 4 bit SD interface in 3V, with MMC1_DAT[7..4] as GPIO.
Can I put vdds_mmc1a at 3.3V to have 3.3V GPIOs ?
Thanks
Philippe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM3730
Hi,
In my design I am using a 4 bit SD interface in 3V, with MMC1_DAT[7..4] as GPIO.
Can I put vdds_mmc1a at 3.3V to have 3.3V GPIOs ?
Thanks
Philippe
Well, a bit of a monologue here... I've found the answer :-)
TRM chapter 7.4.5.1 PBIAS Cells
"With the appropriate configuration of the PBIAS cell, gpio120 through gpio129
I/Os(MuxMode = 0x4) can operate in 3-V mode."
Hi Phillippe,
I am also working on doing this on the DM3730.
Following is the e-mail I dropped to my FAE. If you have some extra info on specifically what needs to be configured and when, I would be highly appreciative.
-----snip--------
I am running into a problem using the TI DM3730 part. We are trying to use GPIO ports 127 & 129 for normal 1.8V GPIO, but these ports are “extended-drain” I/O pins which require extra configuration of “PBIAS” circuitry, which selects between 1.8V and 3.0V output based on input voltage on the SIM_VDDS supply rail. At this point I’ve done all the configuration the data sheet recommends, and I am still not able to use these pins as GPIO. I am noting that the data sheet is not very clear on the use case I’m describing.
My general configuration practice (testing with pin 129):
(CONTROL_PBIAS_LITE[PBIASLITEPWRDNZ1] is 0 to start)
· Set SIM_VDDS supply to 1.8V (The signals are buried, so verifying this electrically this would be tough, but a step that may be necessary)
· Set pin mux to output (no pullup/pulldown)
· Set GPIO output enable for pin 129
· Set GPIO output high for pin 129 (will light an LED when the pin is high)
· Set CONTROL_PBIAS_LITE[PBIASLITEVMODE1] to 0
· Set CONTROL_PBIAS_LITE[PBIASLITEPWRDNZ1] to 1
· Set CONTROL_WKUP_CTRL[GPIO_IO_PWRDNZ] to 1 (not sure if this necessary but I have tested with and without this step)
So far none of this has worked. I have attempted to set the pin in “pull-up” state through the MUX register and notice that it lights the LED in this state but is not controllable by the normal GPIO registers.
Summary: My goal is to have the pins 127 & 129 behave like any other GPIO (‘0’ causes a low state on the output, ‘1’ causes a high state (1.8V) on the output). My problem is that they don’t behave that way and the MCU requires extra configuration to get them to.
Update:
Just found a spot to measure my SIM_VDDS and it looks like that's not set correctly. Looks like I need to address that first. :)