This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Self-Refresh w/256MB of RAM in PM lowest power modes

Has the self refresh mode for the LPDDR been tested with the full 256MB that's in the newer beagleboards and EVMs?

I know that both newer beagleboards and the OMAP-35x EVMs (e.g. Rev.G) have 256 MB of LPDDR on them.  Their POP packages use two LPDDR chips that are each 128MB to create the 256MB in the POP package.

My testing with PM indicate that when mem=99M kernel command-line parameter the system sleeps fine, and wakes up properly after sleeping for several minutes.  If I use the mem=99M@0x80000000 mem=128M@0x88000000 parameters that are suggested in the user guide for 256MB memory, then it doesn't wake up.

Any suggestions for getting self-refresh to work for 256MB?

 

Thanks,

 

Chris