This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uPP Digital Loopback EVMOMAPL138 failure

Other Parts Discussed in Thread: CDCE913

Hi,

I am newbie in upp communication, may be anyone can help me to solve my problem. I try to modify upp example from LogicPD for EVMOMAPL138. I want to transmit signal by channel B and receive signal using channel A using digital loopback UPDLB. But the digital loopback didn't work well. Hereby snippet of the code.

uint32_t TEST_adcdac(void)
{

    uint32_t retVal = ERR_NO_ERROR;

   printf("--------------------------------------------------------------------\r\n");
   printf("                   UPP / ADC / DAC test\r\n\r\n");
   
   printf("Additional Equipment\r\n");
   printf("--------------------\r\n");
   printf("- Oscilloscope\r\n\r\n");
   printf("- Cable with SMA connector\r\n\r\n");
   printf("- Function Generator (passthrough test only)\r\n\r\n");
   printf("- 2nd cable with SMA connector (passthrough test only)\r\n\r\n");
   
   printf("Test Description\r\n");
   printf("----------------\r\n");
   printf("The test will begin producing a 73.2421875KHz sine wave on the analog out line\r\n");
   printf("(left SMA connector). After 20 seconds 64 samples will be collected from the ADC (right \r\n");
   printf("SMA connector). These samples will be output through the DAC for a period of 20 Seconds. \n\r");
   printf("Note that the DAC and ADC are inductively/capacitively coupled with thier connectors.\n\r");
   printf("It is strongly reccomended that the signal provided to the ADC have a freqency that is an \n\r");
   printf("an integer multiple of 73.2421875KHz and below 1.171875MHz.\n\r");

   printf("--------------------------------------------------------------------\r\n\r\n");

   //-------------------------------------
    // initialize the required bsl modules.
    //-------------------------------------
   printf("Initialize the Required BSL Modules\r\n");
   printf("-----------------------------------\r\n\r\n");
   
    //setup UPP
      I2CGPIO_init(I2C_ADDR_GPIO_UI);     //IO expander on UI board
    I2CGPIO_setOutput(I2C_ADDR_GPIO_UI, I2C_GPIO_UI_SELA, OUTPUT_LOW);
    I2CGPIO_setOutput(I2C_ADDR_GPIO_UI, I2C_GPIO_UI_SELB, OUTPUT_LOW);
    I2CGPIO_setOutput(I2C_ADDR_GPIO_UI, I2C_GPIO_UI_SELC, OUTPUT_HIGH);      //UPP now controls ui databus

    //Setup ADC Clock
    CDCE913_setOutput(cdce913_output_2, 6);        //set to 4.5Mhz
    
    //--------------
   // execute test.
   //--------------
   printf("\r\nExecute Test\r\n");
   printf("------------\r\n\r\n");
       
   retVal = executeTest();
   if (retVal != ERR_NO_ERROR)
   {
      printf("ADC/DAC Test FAILED\r\n\r\n");
      return (retVal);
   }
   else
   {
      printf("ADC/DAC Test completed successfully\r\n\r\n");
   }

 return retVal;
}

//-----------------------------------------------------------------------------
// Private Function Definitions
//-----------------------------------------------------------------------------

uint32_t executeTest(void)
{    
    upp_config_t config;
    UPXS2_t    * UPIS2r = (UPXS2_t *)&(UPP->UPIS2);
    UPXS2_t    * UPQS2r = (UPXS2_t *)&(UPP->UPQS2);

      uint32_t retVal = ERR_NO_ERROR;
      uint32_t i;

    //UPCTL
    config.UPCTL.value=0;
    config.UPCTL.bits.IWB = 1;            //16 bit interface
    config.UPCTL.bits.DPWB = 2;            //10 bit data

    config.UPCTL.bits.DPFA = 0;
    config.UPCTL.bits.DPWA = 2;
    config.UPCTL.bits.IWA = 1;

    config.UPCTL.bits.CHN = 1;            //dual channel mode
    config.UPCTL.bits.MODE = 2;            //0 all recv, 1 all xmit, 2 a recv b xmit, 3 a xmit b recv
                                        //Channel A ADC, Channel B DAC

    //UPICR
    config.UPICR.value=0;
    config.UPICR.bits.CLKDIVB = 15;        //Set DAC sampling freqency at 75/16 Mhz (4.6875MHz)

    //UPIVR
    config.UPIVR.value=0;
    config.UPIVR.bits.VALB = 0x1000;
    config.UPIVR.bits.VALA = 0x0000;

    //UPTCR
    config.UPTCR.value=0;                //all values 0 for 64byte DMA bursts read / write
    //UPDLB
    config.UPDLB.value=0;                //no loopback
    config.UPDLB.bits.BA = 1;
    config.UPDLB.bits.AB = 0;
    //UPIES                            
    config.UPIES.value=0;                //dont enable any interrupts
    //UPPCR
    config.UPPCR.value = 0;                
    config.UPPCR.bits.EN = 1;            //enable uPP
    config.UPPCR.bits.RTEMU = 1;        //allow emulator use
    config.UPPCR.bits.SOFT = 1;            //allow emulation
        
    UPP_init(&config);     

    printf("---Generating 73.2421875KHz sine wave for 20 seconds---\r\n\r\n");
    for(i = 1; i < 1464843; i++)
    {
    
            UPP->UPQD0 = (uint32_t)&xmit_buffer;//add next DMA transfer
              UPP->UPQD1 = 0x00010080;               //1 lines 128 bytes per line
              UPP->UPQD2 = 0x00000080;               //no offset between lines

            while(UPQS2r->bits.PEND == 1){};
    }
    
    printf("---Collecting 64 samples from ADC---\r\n");
    UPP->UPID0 = (uint32_t)&recv_buffer;//add next DMA transfer
    UPP->UPID1 = 0x00010080;               //1 lines 128 bytes per line
    UPP->UPID2 = 0x00000080;               //no offset between lines
    while(UPIS2r->bits.PEND == 1){};
    

    printf("---Displaying collected samples---\r\n");
    for(i = 0; i < 1464843; i++)
    {
        UPP->UPQD0 = (uint32_t)&recv_buffer;//add next DMA transfer
          UPP->UPQD1 = 0x00010080;               //1 lines 128 bytes per line
          UPP->UPQD2 = 0x00000080;               //no offset between lines

        while(UPQS2r->bits.PEND == 1){};    //wait for tx transfer to complete
    }

   return retVal;
}