This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM33x DRM driver without TFP410

Other Parts Discussed in Thread: TFP410

I am trying to get the tilcdc panel driver working with the DRM subsystem but without the TFP410. We have the Sitara connected directly to a TFT panel, like on the EVMSK board - but a different panel. When I boot the board, because there is no TFP410 in the device tree the DRM finds no encoders or connectors:

[drm] Initialized drm 1.1.0 20060810

[ 0.983480] Error: Driver 'tfp410' is already registered, aborting...
[ 0.993494] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 0.999902] [drm] No driver support for vblank timestamp query.
[ 1.006064] tilcdc 4830e000.lcdc: No connectors reported connected with modes
[ 1.013105] [drm] Cannot find any crtc or sizes - going 1024x768
[ 1.060119] Console: switching to colour frame buffer device 128x48
[ 1.092459] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.097898] tilcdc 4830e000.lcdc: registered panic notifier
[ 1.133064] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0

Based on this output, I wouldn't expect that the LCD will work - and it doesn't. I assume using the DRM somehow works on the EVMSK, but how? Thanks.