Other Parts Discussed in Thread: OMAPL138
I am moving from a C6748 to an omap L-138 so I can leverage the ARM for extra processing power. I read the documentation on booting up both processors. That is rather straightforward. After they both boot up, do both processors setup:
pin mux settings?
PLL 0 and 1?
power and sleep controller?
If both processors will read from the same EMIF location (an FPGA), will they both setup the chip enables for EMIFA (CE4CFG)?
Or does only one processor setup these and they both use them?