This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3352 pinmux question

So we have our pinmux mostly laid out but there is one thing that is bugging us

we were going to use pin H18 as a gpio pin but in our pinmux we are using McASP1 which is using H18 for AXR3.  for the AXR pins it says to pick any 2 but when we only pick 2 we get a conflict, when we pick all 4 we get a thumbs up.  so when you use McASP1 do you have to pinmux out ALL the pins for that peripheral?  or is there a reason we can't unselect AXR2 and 3 to be able to use those pins as gpio?

attached is the pinmux config file

AM335x 053116.zip