This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

crash happened when connecting HTTP server on TM4C

Other Parts Discussed in Thread: EK-TM4C1294XL

Hi All, 

Would you help me to analyze this crash issue on HTTP server ?

I'm testing HTTP server module with EK-TM4C1294XL board.

I ported example of  http://processors.wiki.ti.com/index.php/TI-RTOS_HTTP_Example.

I have set most of setting for RTOS as document described

I added index.h, efs_stdio.c and add AddWebFiles() at Network IP address hook fucntion. 

only index.h is used for AddWebFiles, no more else.

I boot up the board and try to connect with Chrome broswer on PC(typing "http://192.168.0.14"), then board is crashed

following is system log at crash 

========================

Using MAC address in flash
Network Added: If-1:192.168.0.14
Service Status: HTTP : Enabled : : 000
e: 0x2000f4b0.
Task stack size: 0x800.
R0 = 0x20009ba4 R8 = 0x000197e5
R1 = 0x2000a5a4 R9 = 0x2000aa1c
R2 = 0x00000000 R10 = 0x00000005
R3 = 0x00000000 R11 = 0x00000001
R4 = 0x65646e69 R12 = 0x2000a5c8
R5 = 0x000199b8 SP(R13) = 0x2000fc30
R6 = 0x20018a9c LR(R14) = 0x000023cb
R7 = 0x2000a5a4 PC(R15) = 0x000197ee
PSR = 0x21000000
ICSR = 0x00423803
MMFSR = 0x00
BFSR = 0x82
UFSR = 0x0000
HFSR = 0x40000000
DFSR = 0x0000000b
MMAR = 0x65646e69
BFAR = 0x65646e69
AFSR = 0x00000000
Terminating execution...

=======================

Could you help me to analyze this log and trace the cause of crash ?

or If you need any further information, then just me know, I will try to get it.

Best Regards,

Hae Ryong